Motor_R
Motor_R
| Address: | 8192 (2000H) |
| Type: | DWORD |
| Access: | Read/Write |
| Unit: | mΩ |
| Range: | DWORD |
| Default Value: | 380 |
| Store Supported: | Yes |
| Description: | This object sets the motor R (resistance). This value is used when bit #9 of Drive_Working_Settings_Extended object is equal to 0. |
| Notes: |
-- |